AXIS#.HOME.IPEAK
Description
AXIS#.HOME.IPEAK is the peak current that will be applied when homing against a mechanical stop.
AXIS#.HOME.IPEAK is used when AXIS#.HOME.MODE is 8, 9, 10 or 12.
The current limits AXIS#.IL.LIMITP and AXIS#.IL.LIMITN are set to ±AXIS#.HOME.IPEAK while homing. Once the home position has been found, the current limits are restored before any additional move using AXIS#.HOME.DIST starts.
By default, this value is zero. For the axis to move AXIS#.HOME.IPEAK needs to be set to greater than zero. If AXIS#.HOME.IPEAK is zero and AXIS#.HOME.MODE is 8, 9 or 10, W6026 warning is generated. If the home move is started with this warning, then F6026 fault is generated.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
This content is not applicable to KAS.
|
Type |
Read/Write |
|
Units |
Arms |
|
Range |
0 to AXIS#.IPEAK |
|
Default Value |
0 |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.HOME.IPEAK | 0x5008 | 0x5 | DINT | 1000:1 | - | RW | False |
| AXIS2.HOME.IPEAK | 0x5108 | 0x5 | DINT | 1000:1 | - | RW | False |
Related Topics
Homing